Encoder Emulation
RON TO PROVIDE TEXT.
Element | Property | Description | Parameter | |
---|---|---|---|---|
Encoder Emulation Source |
![]() |
Feedback source |
This parameter sets the position source used to drive the EEO generator. 1 – Feedback 1 3 – Feedback 3 4 – Feedback 4 5 – Feedback 5 |
|
Configure Zero Pulse![]() |
![]() |
Zero Pulse Mode - Once per revolution | This parameter sets the position within each revolution where the Z pulse will be generated, when the one Z pulse per rev mode is selected (EEO#.ZMODE 0) | EEO#.ZOFFSET |
Zero Pulse Mode - Absolute position | This parameter sets the position of the Z pulse when the absolute Z pulse mode is selected (EEO#.ZMODE 1). | EEO#.ZP | ||
Encoder Emulation Output Generator |
![]() |
Mode |
This parameter specifies the type of output waveform an EEO generator will create. 0 – A Quad B 1 – CW/CCW 2 – Step/Direction |
EEO#.MODE |
Lines | 1.000 | EEO#.LINES | ||
Pulse Width | 4.0800000 | EEO#.PULSEWIDTH | ||
X23 |
![]() |
Shows feedback and selecting will take you to the Hardware Configuration. |